AnsweredAssumed Answered

LPC11U68 ADCs 2Ms/s

Question asked by Bob Bann on Jul 20, 2016
Latest reply on Aug 22, 2016 by Kerry Zhou

LPC11U68 ADCs claim to run at 2Ms/s, but I am seeing conversion times of >60 clock cycles at 48MHz (<1Ms/s). I'm running a SeqA with a single channel in Burst mode, with an IRQ handler in RAM reading results into a simple buffer. Can anyone point me at a code sample which can achieve the 2Ms/s. I've checked the clock divider is 0 and Vdda is 3.3V.

 

Cheers, Bob.

 

EDIT :

 

  I solved this issue using DMA. 2MHz was then achievable.

Outcomes