I used to use CW version 6.3.1 in order to compile code for a MC9S08JM60 microcontroller. Since this version of CW is not supported by Windows 7, I had to start using CW for MCU 10.6.4 (which is Eclipse-based). I do not mind and I have figured out how to set up and compile my project. The only thing is that I cannot see the code size for the project. The older version of CW showed the size of the project (and of each individual file/module).
How can I see the code size using the new tool?
Hi Daniel,
I hope this helps,
Erich
(The "Cross ARM GNU Print Size" option does not exist under the "Tool
Settings" tab.)
Hi Daniel,
if you have CW for MCU 10.6.4 installed with the ARM tools, then it comes with the size utility.
You can use it as described here: https://mcuoneclipse.com/2014/05/04/printing-code-size-information-in-eclipse/ with a 'post build' action.
The thing is that the S08 tools produce the .abs file which is a ELF/Dwarf file, which can be consumed by the size tool.
I hope this helps,
Erich
Erich,
Thank you for the information. Unfortunately, it does not work for me
as the version of CW for MCU 10.6.4 I am using does not have that
option. It's not an ARM micro but an MC9S08JM60 micro.
Thank you
Daniel