AnsweredAssumed Answered

QSPI control of the WP signal to restore flash lock up

Question asked by Luc Roy on Jul 20, 2016
Latest reply on Jul 21, 2016 by Serguei Podiatchev

We are using the ls1021iot board with the s70fl01gs nor flash on board.

The SDWD, BP0-2 bits of the status register of the s70fl01gs were inadvertently set to one and are stuck in that mode. Power cycle does not restore the flash.

 

The s70fl01gs document specifies the following:

If WP# signal (according to IOT schematic: LS1021 pin C12, label IFC_A24/QSPI_DIO_A2/IFC_WP3) is high the SRWD bit and BP bits may be changed by the WRR (Write Register) command.

 

Is it possible to control the WP# signal of the QSPI device while sending a message (WRR: Write Register) to the s70fl01gs nor flash?

Outcomes