about SSI timing of i.mx6dl

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about SSI timing of i.mx6dl

302 Views
宗標廖
Contributor V

Hello,community

I referred to datasheet of i.mx6dl about SSI timing.

pastedImage_0.png

In table 87,  the min values of SS24,SS26,SS37~SS39 are not specified.Does it mean that these values have no lower limit(Can be a minus value)?

It seems that it is not reasonable for SS24,SS26 having a minus value.

Thank you!

ZongbiaoLiao

Labels (1)
0 Kudos
1 Reply

256 Views
art
NXP Employee
NXP Employee

Actually, the minimum limit for these parameters you've listed is 0. And, you are right, they can't have a negative values.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos