Is the LS1046A or LS1026A accessible as part of embedded system on module?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the LS1046A or LS1026A accessible as part of embedded system on module?

827 Views
kostiantynstaro
Contributor I

I'm interested use in my telepresence project the Cortex A72 processor, but to achieve the project lead time as short as possible I search the ready for purchase solution like system-on-module . If you can suggest the such soulution on base your LS1046A or LS1026A please let me know.

0 Kudos
1 Reply

580 Views
alexander_yakov
NXP Employee
NXP Employee

The LS1046/LS1026 family devices are quite new - we expect first LS1046-based development board will be available at the end of September, 2016.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos