AnsweredAssumed Answered

T4240: SRIO: Why only can see one SRIO controller by CW?

Question asked by carl peng on Jul 15, 2016
Latest reply on Aug 1, 2016 by Yiping Wang

Hello,

 

Why only can see one SRIO controller by CW?

When I used CW to connect to board and see the register of T4240, I curiously find that there is only one

SRIO controller is listed out, then where is the other SRIO controller?

Below is the CW figure related to T4240 registers:

From the upper figure, we can only find one SRIO controller, but from the T4240 spec, should has

two SRIO controllers.

In the figure, should list as below:

SRIO1

SRIO2

Why here only list one SRIO controller? Does it need to do some configuration to enable the other one?

Could you please help to give some suggestions?

 

Thanks a lot!

Carl

Outcomes