PCIE Setup for Sabre board I.mx6sx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIE Setup for Sabre board I.mx6sx

819 Views
stuff
Contributor II


Hey i need to set up a quick way to use the PCIE section on the sabre board that utilizes the i.mx6sx.

Is there a simple way to do this?

sorry for such a newbe question.

Thanks in advance.

Labels (1)
0 Kudos
1 Reply

520 Views
igorpadykov
NXP Employee
NXP Employee

Hi Garrick

PCIe usage is described in attached Linux Manual sect.40.4.2 Tests

and below links

https://community.nxp.com/docs/DOC-95014

https://community.nxp.com/message/623824#comment-623824

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos