Hi, we are using QorIQ T4240 processor, we used 2 pcs SPI flash to store rcw and uboot file, T4240 read rcw configurations and boot from SPI device. we design two spi flash, one is active device, another is backup device, when active device image was bad,

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, we are using QorIQ T4240 processor, we used 2 pcs SPI flash to store rcw and uboot file, T4240 read rcw configurations and boot from SPI device. we design two spi flash, one is active device, another is backup device, when active device image was bad,

606 Views
kentli
Contributor I

Hi, we are using QorIQ T4240 processor, we used 2 pcs SPI flash to store rcw and uboot file, T4240 read rcw configurations and boot from SPI device. we design two spi flash, one is active device, another is backup device, when active device image was bad,we hope it can auto switch to backup device. now we erase one SPI flash all contents, another flash is ok, but CPU can't recover it from another flash, no any output from console port, the hreset signal always keep low. when T4240 can't get rcw and uboot successfully, the problem is reasonable?

Labels (1)
0 Kudos
1 Reply

364 Views
bpe
NXP Employee
NXP Employee

PBL initializes eSPI controller as specified in T4240RM, Section 5.4.10. There are no provisions for backup RCW

or automatic switchover between chips or interfaces.


Have a great day,

Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos