MK24FN1M0VDC12 Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK24FN1M0VDC12 Support

604 Views
tomvandenbon
Contributor I


Hi There,

How difficult would it be to add support for MK24FN1M0VDC12? There is support for MK24FN1M0M12, but using my chip it says no matching device (680E0078). Would it be as simple as just adding an entry with the right id?

Thanks,

Tom

Tags (1)
0 Kudos
1 Reply

315 Views
pgo
Senior Contributor V

Hi Tom,

The IDs I use in the C:\Program Files (x86)\pgo\USBDM 4.12.1.120\DeviceData\arm_devices.xml file is usually based upon the description in the if I don't have a sample.

I would expect the chip to program as a MK24FN1M0M12 - Perhaps I have the ID wrong.

Try opening the above file and adding another SDID Line with the number of your chip e.g.

     <sdid value="0x680E0078" mask="0xFFF00F80"/>
    

Let me know if this works.

bye

0 Kudos