Hello,
I have a uLinkPro (without 'D') from a previous ARM Cortex-M4 project with KEIL uVision.
Now using i.MX6. Can the debugger be re-used? Can uVision still be used for it?
Or must I use DS-5?
I already installed and tried to get DS-5 up and running,
but found no hint/reference to uLinkPro, only e.g. DStream, (remote) gdb.
How can it be used? Is there some configuration menu? Some additional software needed?
Is there some example, which shows how to use it together with IMX6?
Best regards,
Martin
Hi Martin
seems it can be used with Cortex A9, i.MX6 as discussed on:
https://community.arm.com/thread/4987
https://community.arm.com/thread/5736
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------