使用IMX6Quad的imx6q-sabresd平台,BSP为L4.1.15-1.0.0的版本,是带QT的linux系统,而不是android。如何实现同时从lcd和lvds输出相同内容?能简单通过boot参数来设置么?有相关的文档参考,或者具体的步骤么?
你好
我也遇到了相同的问题,用的内核和您的一样,请问您的问题解决了吗?
开机启动的时候 logo只在fb0上显示,不在fb1显示。请问您是怎么解决的呢?
谢谢
Hi yang,
The linux BSP on imx6q-sabresd do not support dual screen display at the same time. But the android BSP support, and you just need to configure the boot command in u-boot, it can work.
Here you need to output the same on the lcd and LVDS screen, you mean play videos or ...? Could you please describe it in details?
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi,Dan
firstly,thanks for your help.I want to play video on the LVDS and LCD.If i do that,how to do?