AnsweredAssumed Answered

Whats is the meaning of these variables?

Question asked by Carlos Lavín on Jul 8, 2016
Latest reply on Jul 27, 2016 by Jorge_Gonzalez

static uint8_t sens_res[2] = { 0x04, 0x00 };  /* ATQ bytes - needed for anti-collision */

static uint8_t nfc_id1[3] = { 0xA1, 0xA2, 0xA3 };  /* user defined bytes of the UID (one is hardcoded) - needed for anti-collision */

static uint8_t nfc_id3 = 0xFA;  /* NFC3 byte - needed for anti-collision */

static uint8_t poll_res[18] = {

  0x01, 0xFE, 0xB2, 0xB3,

  0xB4, 0xB5, 0xB6, 0xB7,

  0xC0, 0xC1, 0xC2, 0xC3,

  0xC4, 0xC5, 0xC6, 0xC7,

  0x23, 0x45 };  /* felica - needed for anti-collision */

 

 

It appears in the basic loop discovery example for the NXP NFC library...

 

I was not able to understand them...

 

Can you help me, please?

Outcomes