AnsweredAssumed Answered

K64F demo boards and the MULT2-B shield. Demo will not run

Question asked by george evans on Jul 8, 2016

After loading drivers per quick start quide it is not posible to run the outofbox demo and two of the boards do not flash the RGB LED only one does.  

 

Also only 6 projects apear listed and non of them run and the important sensor fusion package is missing . Where can the missing packages be downloaded? After loading drivers per quick start guide it is not possible to run the outofbox demo and two of the boards do not flash the RGB LED only one does. Also only 6 projects appear listed and non of them run and the important sensor fusion package is missing . Where can the missing packages be downloaded?   I also want to evaluate the 6 and 9axis e-compass and need help with using Codewarrier.

Outcomes