NFC Class 6 Antenna Design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Class 6 Antenna Design

3,503 Views
davidcrosby
Contributor I


Is there are reference design for a Class 6 antenna on standard 0.062" thick FR4 material? I have seen a Class 6 flex circuit reference design only.

0 Kudos
1 Reply

1,985 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello David Crosby:

You might want to take a look to the NTAG Antenna Design Guide ZIP package (which includes the AN11276 application note). The ZIP is available from the next link and it includes reference Class6 antennas:

NTAG I2C plus |Connected NFC Tag with I2C Interface|NXP

Basically the same design should work either on PCB or in a Flexible material, as long as there a no metal surfaces in the surroundings.

I hope this helps.


Best Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos