AnsweredAssumed Answered

Sequence of commands to obtain UID in PN5180

Question asked by Alicia Hurtado on Jul 7, 2016
Latest reply on Jul 25, 2016 by Jorge_Gonzalez

Hi all,

 

We have develop a new prototype in which we have added PN5180 NFC Chip.

I am having difficulties in finding documentation regarding communication between host and chip PN5180 by SPI interface. I have found document PN5180 v2.2 in NXP and the library NFCReaderLibrary (v4.010.03.001609_R1.2).

 

My concern is that this library seems not to support our MCU.

I would be pleased if you could provide help regarding which is the specific sequence of commands (from document PN5180 v2.2) that we need to send to PN5180  in order to obtain UID for a card (ISO/IEC 14443A) like NTAG213 that we use.

Outcomes