AnsweredAssumed Answered

MPC5748G Nexus Connector

Question asked by Steve Lyon on Jul 6, 2016
Latest reply on Jul 11, 2016 by Steve Lyon

Hi, could I get confirmation of the Nexus connector part number used on the MPC5748G eval board?

 

I found AN4224:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN4224.pdf

 

which says the recommended 50 pin connector is the Samtec ASP–148422–01, but I could not find any stock of that part at any distributor.

Is that the part to use or should I transition to one of the other suggested connectors?

Our Green Hills debugger connects fine to the Nexus connector on the eval board so I wanted to use the same one on our dev board we will eventually make so wanted to make sure I am using the correct connector that I can actually get.

 

Thanks,

Steve

Outcomes