I am going to develop a engine management ECU based on the S12XE. I have bought the KIT33812ECUEVME Small Engine Control and have studied the code. This has been helpful.
I am looking to another code example that will give me a deeper understanding of how to achieve the best engine control.
Ray.
Hi Ray,
i found a project based on S12P device for a scooter which has a two-cylinder engine i suppose.
Not sure if this can be of help to you, but the actual problem i see if we can share this with you at all.
Maybe it would work with some NDA.
Regards,
iggi
Hello Iggi,
Is this the project from the freescale Small Engine Control KIT33812ECUEVME. If it is, then I have that code as I bought the kit. If not, then I would be intrested in seeing the code. Maybe email it to me if posible,
Ray.
The project i found (under different name) is the same as KIT912S812ECUEVM_Project.zip delivered with the kit. I compared the source files and there is no difference.
It looks like there are no other codes/projects related with this kit for studying.
Regards,
iggi