Is some spec of MMPF0100 buck regulator changed when changed SWx_PWRSTG[2:0]?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is some spec of MMPF0100 buck regulator changed when changed SWx_PWRSTG[2:0]?

Jump to solution
942 Views
satoshishimoda
Senior Contributor I

Hi community,

Our customer have a question about MMPF0100.

Please see chapter 6.4.4.2.3 in MMPF0100 datasheet.

They want to know whether some specification of buck regulator is changed when change the current configuration SWx_PWRSTG[2:0].

For example, set SW2_PWRSTG[2:0] from 2.0A to 0.75A when the load current is 200mA.

In this case, is some specification (efficiency, duty, etc...) change?

Best Regards,

Satoshi Shimoda

Labels (1)
Tags (1)
0 Kudos
1 Solution
674 Views
art
NXP Employee
NXP Employee

The setting of the SWx_PWRSTG[2:0] bits just change the number of FETs working in parallel to drive the inductor. In the case you describe (SW2 is set for 0.75A max. load whereas the actual load current is 200mA) no changes in efficiency or other SW2 parameters will occur.


Have a great day,
Artur
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
675 Views
art
NXP Employee
NXP Employee

The setting of the SWx_PWRSTG[2:0] bits just change the number of FETs working in parallel to drive the inductor. In the case you describe (SW2 is set for 0.75A max. load whereas the actual load current is 200mA) no changes in efficiency or other SW2 parameters will occur.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos