Hi ,
I am currently facing some problems with mxc_v4l2_tvin.out test in IMX6Q sabrelite. My system configuration is as follows:
1. LTIB version : L3.0.35_4.1
2. Ubuntu 14.04
Problem:
I am interfacing adv7180 decoder to the sabrelite card through IPU0->CSI0, the drivers are loaded properly, then when i run mxc_v4l2_tvin test the output the output is also displayed on the screen; but after some time the output gets blank. So pls provide some suggestions to overcome the issue.
Regards,
Vignesh
Hi Vignesh
please try to disable blanking
Disable screen blanking on i.MX6 running Yocto | NXP Community
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------