Hello,
I added the following description in /conf/local.conf.
EXTRA_IMAGE_FEATURES = "tool-debug"
After that I was able to use gbd and gdbserver of the 7.7.1 version.
Now I'd like to use 7.1 version and how can I get the older version of gdb installed?
Regards,
Sho
Hello Shoji Goto
There may be a different version of gdb depending on the BSP you are using but this package is part of the open embedded layer so you may be able to import the recipe from an older release of the Open Embedded layers. However, you would need to be careful with the dependencies for the older version as there may be conflicts.
Regards,