Description in i.MX6DQRM between Rev.2 and Rev.3 about μSDHC.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Description in i.MX6DQRM between Rev.2 and Rev.3 about μSDHC.

Jump to solution
743 Views
keitanagashima
Senior Contributor I

Dear All,

Hello.

Refer to 67.2 External Signals in IMX6DQRM(Rev.2).

The uSDHC4 signals exist.

But, the refer to 67.2 External Signals in IMX6DQRM(Rev.3), the uSDHC4 signals wasn't seen.

Is this typo?

Best Regards,

Keita

Labels (2)
1 Solution
616 Views
Yuri
NXP Employee
NXP Employee

Sorry, my misprint : the section 67.2 in the RM, rev.3 is not full.

View solution in original post

0 Kudos
5 Replies
616 Views
Yuri
NXP Employee
NXP Employee

OK !

0 Kudos
616 Views
Yuri
NXP Employee
NXP Employee

Hello,

i.MX6 DQ supports uSDHC4 port; so, the section 67.2 in the RM, rev.2 is not full.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
616 Views
keitanagashima
Senior Contributor I

Hi Yuri,

>i.MX6 DQ supports uSDHC4 port; so, the section 67.2 in the RM, rev.2 is not full.

No.

RM rev.2 was descripted about uSDHC4.

In RM rev.3, the description was lost.

Best Regards,

Keita

0 Kudos
617 Views
Yuri
NXP Employee
NXP Employee

Sorry, my misprint : the section 67.2 in the RM, rev.3 is not full.

0 Kudos
616 Views
keitanagashima
Senior Contributor I

Hi Yuri,

OK. I think so, too.

Thank you very much.

If NXP has the plan of document update, please fix the typo.

Best Regards,

Keita