I want to do a compatibility design with K20P100M72SF1 and K22P121M100SF9. The K20 has an inner USB regulator, but K22 not. The pin G3 of K22 is USBVDD, and K20 is VOUT33. In my design, i donot need the USB Vbus to supply for the device. I'm not sure whether can I directly connect the pin G3 to the 3.3V for K20?
Solved! Go to Solution.
Hi Li Wang,
Yes, I think so, as the VDD and pin G3 ( USBVDD or VOUT33 ) both are connected in the above figures.
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
OK, thanks.
Just because the datasheet does not mention about it. I want to confirm it.
Hi,
Even had a brief look through the statement above, I'm afraid of not get the totally understand of your question.
So I was wondering if you can share the sch of your design and clarify the question again.
I'm looking forward to your reply
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
K20P100M72SF1, it has an inner USB regulator.
K22P121M100SF9, it need an external regulator.
Can i design the schematic like K22 figure shown above? Then i can choose either K20 or K22.
Hi Li Wang,
Yes, I think so, as the VDD and pin G3 ( USBVDD or VOUT33 ) both are connected in the above figures.
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------