Hi Erich!
I'm using your component module WAIT1 at KL25Z. When I use with "Internal Oscillator" works well, but when is configured for External Crystal the delays are divided by 2. Can you help me?
Note: Component Inspector - Cpu
System oscillator 0 --> Enable
MCG mode --> PEE
MCG output[MHz] --> 96.0
Core clock --> 48.0
Bus clock --> 24.0
Regards,
Arnaldo
Hi Arnaldo,
For me, the delay time are around 10 ms both for the internal clock and the clock configuration you have. Keep in mind that because it is using a number of nops to wait, the timing is in the ~10% range.
Below is the code for toggling the blue LED (PTD1) on the FRDM-KL25Z:
Default internal clock:
With your clock settings:
The number of wait cycles is based on the core clock:
Which 48MHz in that configuration:
I know there was an issue with what clock to be used (it used the bus clock instead of the the core clock) in a very old Wait component (about 2 years ago).
Are you really using the latest version from SourceForge (see https://mcuoneclipse.com/2014/10/21/mcuoneclipse-releases-on-sourceforge/ )?
In any case, I have attached my test project so you can compare the code and component version numbers.
I hope this helps,
Erich
PS: I recommend to report issues in the GitHub tracking system here: Issues · ErichStyger/McuOnEclipse_PEx · GitHub