T1040 Voltage Ramp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1040 Voltage Ramp

419 Views
darrellblock
NXP Employee
NXP Employee

Customer has T1040 power-up question.  They are planning on having all voltage rails come up ratiometrically (see image).  This looks to be OK but they would like verification.


T1040 Voltage Ramp.png
   
 
 
 
 
 
 
 
 
 
 
 





Labels (1)
Tags (1)
0 Kudos
1 Reply

323 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The T1040 data sheet available on the NXP site (link) provides  the power sequencing requirements. It should be satisfied. There are 3 groups of power supplies. There is not ordering requirement with respect to one another in the same group. Groups 1,2 and 3 must be ordered sequentially such that voltage rails on a previous step must reach 90% of their value before the voltage rails on the current step reach 10% of theirs

Ramp-up.png

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos