PCA8565 can't work to 125 ℃

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA8565 can't work to 125 ℃

686 Views
liushuo1
Contributor I

     When PCA8565 work at 90~125℃,CPU can't read the true time from PCA8565.But the timer in the PCA8565 is working normally.When the temperature drops below 90℃,PCA8565 return to normal working condition.

        The circuit diagram as follow.

        All chips and devices can work at 125 ℃.What factors will cause this error?

QQ截图20160629095438.png

The correct data:

pastedImage_4.png

The wrong data:

pastedImage_6.png

Tags (1)
0 Kudos
2 Replies

537 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Shuo,

First off, please accept our apologies for this delayed response.

A few questions to let us start looking into it:

1. Crystal CL?

2. Measure the 32.768kHz at the CLKOUT pin (need an external pull-up).

3. Values of Control registers?

Best regards,

Tomas

0 Kudos

537 Views
liushuo1
Contributor I

I took off all resistors and capacitors,leave only PAC8565 and crystal.

Like this:

QQ截图20160719085633.png

Then the part of clock can work normally until 125℃.

  • SO can I use this circuit?I'm afraid it will have other error in the future.
0 Kudos