AnsweredAssumed Answered

Support for DPAA1

Question asked by Ram Krishnan on Jun 28, 2016
Latest reply on Jun 29, 2016 by bpe

This is a question regarding DPAA1 and DPAA2. If I am to decide on a chipset primarily used for network packet processing, is it better to wait for a chipset that supports DPAA2 or go with the T4240 which supports DPAA1. Will the DPAA1 go away and be replaced with DPAA2. It is also nice that the DPAA2 has the ODP support. I also see that some demo applications that were supported on the older SDK's are not there anymore on the newer 1.9 and 2.0 SDK's. Any recommendations will be helpful..

 

Regards,

Ram

Outcomes