Can T1024 be configured for PCIe 1.0 x4 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can T1024 be configured for PCIe 1.0 x4 ?

483 Views
sarojbharti
Contributor I

Can T1024 be configured for PCIe 1.0 x4 ?

Labels (1)
0 Kudos
1 Reply

355 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Yes the T1024 can be configured for x4 link width at PCIe Gen1 (2.5 GT/s) speed.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos