Hi,
I want to use Dstream DSTREAM – ARM Developer for debugging along with LS1021A rev:2.0, I am using a 10 pin JTAG connector for connection at J12 connector. Is it correct connector ?
In Dstream case K20 JTAG connector should not be used ?
Any pointers or references will be a great help!
Thanks
Shrikant
Solved! Go to Solution.
Is your request about the TWR-LS1021A board?
If "yes", then J12 has to be used for the debugger connection.
Which NXP board is in question?
Please note that we do not support third-party tools.
Hi,
Board in question: Layerscape 1021A rev 2.0: QorIQ LS1021A Dual-Core Communications Processor wi|NXP
Thanks for an update.
Thanks
Shrikant
Is your request about the TWR-LS1021A board?
If "yes", then J12 has to be used for the debugger connection.
yes, TWR-LS1021A board, Thanks for confirming the J12 JTAG connector.
Thanks
Shrikant