AnsweredAssumed Answered

FlexCAN CRC Issue

Question asked by Nathaniel Hinshaw on Jun 23, 2016
Latest reply on Jun 24, 2016 by Nathaniel Hinshaw

Hello, I was working on my K64F board, and noticed an oddity.  the other controllers on the network, using MSCan interfaces, werent picking up any of the traffic from my K64F.  I hooked into a logic analyzer and noticed that the CRC generated from the K64F was different than the CRC generated from a duplicate send from both a KE06Z and a Pcan module, both of which had the same message.  Attached is an image of the Logic analyzer tests.  Is there an issue with the CRC generation on the FlexCAN code, or did I just miss a register somewhere?  Any help would be appreciated.

 

-Nate Hinshaw

Attachments

Outcomes