What are the preferred connections for unused pins one K20DX256V?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What are the preferred connections for unused pins one K20DX256V?

420 Views
elizabethamyoun
Contributor I

What are the preferred connections for unused pins one K20DX256V?

Labels (1)
0 Kudos
1 Reply

248 Views
soledad
NXP Employee
NXP Employee

Hello Elizabeth,

For the Kinetis family it is recommended to leave unused pines floating and configure them as disabled.

In the below document you can find some tips and tricks to consider when designing for low power.

https://developer.mbed.org/media/uploads/GregC/an4470-using_low-power_modes_with_kinetis_mcus.pdf

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos