AnsweredAssumed Answered

Strange MMC boot behavior

Question asked by ROBERT WOOD on Jun 22, 2016
Latest reply on Jun 28, 2016 by Yuri Muhin
  1. On our iMX6DL board we have a Micron MTFC4GACAJCN-4M IT, eMMC device on uSDHC3, which is DDR and byte capable. When configuring for boot, we find the processor boots when the CONFIG2(7:5) field is set to "111" or "010" but not to "110".  Now the reference manual states in Table 5-6

 

Bus Width:

 

000 - 1-bit

 

001 - 4-bit

 

010 - 8-bit

 

101 - 4-bit

 

DDR (MMC 4.4)

 

110 - 8-bit DDR (MMC 4.4)

 

Else - Reserved

What are we doing wrong or right

 

 

Outcomes