Hello,
Why most of the MPC5744P examples are made in CW if this platform do not support this micro? Will it be possible to use CW for this micro in next future?
And has anyone migrated these examples to S32?
Thanks,
Maite
Hi Maite,
where did you find the information that the most examples for MPC5744P is made in CodeWarrior? This platform does not support MPC5744P and It will not be possible to use it in future. There is S32DS from NXP, which supports MPC57xx microcontrollers.
But if you look at the following link, where the most of examples is stored, you will find, that these examples are created in Multi IDE from GHS or in S32DS.
So please check, and write me back if you need more information.
Regards,
Martin
Hi Martin,
Sorry but I was wrong: I assumed that they were created in CW.
Many thanks!
Maite
De: b55689
Enviado el: miércoles, 22 de junio de 2016 14:08
Para: Sierra Bustamante, María Teresa
Asunto: Re: - Examples for MPC5744P in S32?
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Examples for MPC5744P in S32?
reply from Martin Kovar<https://community.nxp.com/people/b55689?et=watches.email.thread> in MPC5xxx - View the full discussion<https://community.nxp.com/message/804531?et=watches.email.thread#comment-804531>