KIT 33908 MBEVBE for KTMPC5744DBUG Daughter board example in S32?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KIT 33908 MBEVBE for KTMPC5744DBUG Daughter board example in S32?

1,023 Views
maitesierra
Contributor II

Hello,

 

"MPC5744P-MC33907-MC33908 Demo Code" example is available in web for KIT33908MBEVBE with KTMPC5744DBUG evaluation daughter board. It contains basic drivers. But it seems to be made in Green Hills. Is it posible to get this example for S32?

 

Thanks in advance.

Maite

Labels (1)
2 Replies

776 Views
martin_kovar
NXP Employee
NXP Employee

Hi Maite,

unfortunately, this example is not is not ported for S32DS. But you have source codes available and there is no obstacle to port it for S32DS.

Regards,

Martin

776 Views
maitesierra
Contributor II

Hi Martin,

Ok, thanks for information.

Regards,

Maite

De: b55689

Enviado el: miércoles, 22 de junio de 2016 13:58

Para: Sierra Bustamante, María Teresa

Asunto: Re: - KIT 33908 MBEVBE for KTMPC5744DBUG Daughter board example in S32?

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

KIT 33908 MBEVBE for KTMPC5744DBUG Daughter board example in S32?

reply from Martin Kovar<https://community.nxp.com/people/b55689?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/804485?et=watches.email.thread#comment-804485>

0 Kudos