AnsweredAssumed Answered

Is there any posibility to use the NTAG I2C Explorer Kit without having to flash the firmware with the LPCLink2?

Question asked by Do Hfr on Jun 23, 2016
Latest reply on Jun 26, 2016 by Jorge_Gonzalez

Hello Everyone. I just wanted to ask if there is a posibility to use the NTAG I2C Explorer Kit without having to flash the firmware with the LPCLink2 or if there are other ways to flash it instead of using the LPCLink2.

Outcomes