I am using FreeRTOS from the Kinetis SDK 1.3.0. A snippet of my code is provided below. Why is the second call to xSemaphoreTakeFromISR() not blocking and not waiting for xSemaphoreGiveFromISR() to release the binary semaphore? If I disable xSemaphoreGiveFromISR() from within IRQHandler_A(), my code within IRQHandler_B() will still move to the next instruction.
void IRQHandler_A(void)
{
…..
xSemaphoreGiveFromISR(Sem, NULL);
…..
}
void IRQHandler_B(void)
{
static bool once = true;
if(once)
{
xSemaphoreTakeFromISR(Sem, NULL); // first time
once = false;
}
…..
xSemaphoreTakeFromISR(Sem, NULL);
// next instruction
…..
}
Hi, Momir,
From instinct, it seems that xSemaphoreTakeFromISR() should not appear in an interrupt service routine as Erich said, how about creating a task, and put the xSemaphoreTakeFromISR() in a forever loop in the task.
I am not sure if the xSemaphoreTakeFromISR() can appear in an ISR, it is only my opinion, pls refer to the FreeRTOS website:
Hope it can help you.
BR
XiangJun Rong
FYI, the *FromISR() functions should be called only from an interrupt service routines.
From a task the xSemaphoreTake() API has to be called.
Erich
Hi Momir,
see This page describes the xSemaphoreTakeFromISR() RTOS API function . Taking a semaphore in an interrupt is not (and should not!) block. Blocking in a semaphore would be a very, very bad thing anyway.
If you need to know if the semaphore was available, you can check the return value of xSemaphoreTakeFromISR() (see above lik to the documentation).
I hope this helps,
Erich