FT5X06 touchscreen on imx6q-sabresd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FT5X06 touchscreen on imx6q-sabresd

734 Views
pengxingwei
Contributor III

hello,

       recently,I also do some work about FT5X06,my IC is FT5506 ,the kernel of my Android system is linux-3.0.35 ,but  the screen can't work ,there is no reflect when I touch the screen ,then I checked it ,it seem that  the interrupt  of touch ic has problem  .the some files or message as follows:

154051_154051.pngpastedImage_0.pngout

can you give me some advice about this? Thank you !

Labels (2)
0 Kudos
2 Replies

405 Views
igorpadykov
NXP Employee
NXP Employee

Hi peng

please look at FT5X06 and touchscreen links

https://community.freescale.com/thread/293210

https://community.nxp.com/message/624165

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

405 Views
pengxingwei
Contributor III

hello,I want to kown whether the SD1_CMD/GPIO1_IO18 pin can use as the interrupt pin.pastedImage_0.png

0 Kudos