AnsweredAssumed Answered

LPC812: Code size too large

Question asked by Fco. Javier Rodriguez G on Jun 20, 2016
Latest reply on Aug 3, 2016 by Rian Malcovich

Hi, while working with the LPCXpresso 812MAX I observed that the code produced for the blinky project is 5532 bytes, too mucho for such a small project (with no optimization at all), but the Board and Chip libraries are set to -Os because no one is going to debug any of them. Is that figure normal for that project?

Captura de pantalla de 2016-06-20 22:56:05.png

Outcomes