TSS(Touch Sensing Software) library migration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TSS(Touch Sensing Software) library migration

Jump to solution
729 Views
kigerzhang
Contributor III

Dear Expert,

Now a cold storage control project  used the S12ZVC  MCU .  It is also required the touch sensing UI .

I want to know   is there possible  to migrate the TSS library  to S12ZVC ?

If it can't be migrated,   please recommend a   industrial or automotive grade MCU. The MCU must has CAN and  ADC (best  if the ADC  there is  program gain control).

Best Regards,

Kiger

1 Solution
425 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Kiger,

The TSS is no longer recommended for new designs and there are no plans to add support for S12ZVC devices. There is a new software library – the NXP Touch Software supporting most of the Kinetis MCUs. The Kinetis E series might be a good choice, but the TSI module is available only on the KE1xZ which does not have the CAN module. So I would recommend considering our standalone touch/promixity sensors which can be connected to the S12ZVC through the I2C.

I hope it helps.

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

View solution in original post

2 Replies
426 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Kiger,

The TSS is no longer recommended for new designs and there are no plans to add support for S12ZVC devices. There is a new software library – the NXP Touch Software supporting most of the Kinetis MCUs. The Kinetis E series might be a good choice, but the TSI module is available only on the KE1xZ which does not have the CAN module. So I would recommend considering our standalone touch/promixity sensors which can be connected to the S12ZVC through the I2C.

I hope it helps.

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

425 Views
kigerzhang
Contributor III

Dear Tomas,

Thank you so much for your help!

0 Kudos