Hi all,
for imx6q-plus have to decide if to use 3.14.52 or 4.1.15.
We actually uses 2 screens, with a 2D app in one + a 3D app in the second.
I am not sure if is more mature the (34.1.14) p8.4 vivante driver compared to p7.4 (3.14.52).
And, it there is any other reason to prefer one or the other.
Many thanks
angelo
Solved! Go to Solution.
Hi Angelo
please refer to attached L4.1.15 Release Notes Table 9 New features
describing new features and bug fixes for the graphics provided in this release,
compared with L3.14.52 previous version.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Angelo
please refer to attached L4.1.15 Release Notes Table 9 New features
describing new features and bug fixes for the graphics provided in this release,
compared with L3.14.52 previous version.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor, many thanks !
I have kernel 4.1.15 running, once added vivante gpu libraries (5.1.1 p8.3) 3D and 2D demos works fine.