TJA1100 dimensions of capacitances of the PI-filters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1100 dimensions of capacitances of the PI-filters

770 Views
jerrry
Contributor II

Hi NXP-community,

I have a question about the PI-filters and their dimensions of the capacitances.

In the application-hints of TJA1100 there are shown two figures, firure 6 and figure 13.

The capacitance right to the supply coming from the LDO, what is the dimension? Are them the 22µF shown in figure 13 or not? So if they are, then my PI-filter will be build this way:  supply(3V3) -> cap(22µ) -> ferrite -> cap(470n) ? (f.e.VDDA(3V3)).

Am I correct? So I only unsure aboiut the cap after the LDO.

Thanks in advance.

Jerrry

Labels (1)
0 Kudos
2 Replies

522 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jerome,

Yes, the 22uF electrolytic capacitor at the voltage regulator output is recommended to reflect the buffering needs of the TJA1100. A higher value may be needed when also considering the buffering needs of your MCU.

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.

522 Views
jerrry
Contributor II

Hi Tomas,

thank you for your response. I added a PI-filter to every supply pin and dimensioned the capacitance for every filter input 10µF. Summed up I now have a bit more than the recommended 22µF. So for every pin (instead of the 1V8) this PI setup (LDO -> 3V3 -> cap(10µF) -> ferrite -> cap(recommended).

Thanks again and best regards.

Jerrry

0 Kudos