P4080: 36bit address: How to use these address space beyond 4GB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P4080: 36bit address: How to use these address space beyond 4GB?

373 Views
carlpeng
Contributor II

As we know, P4080 is E500MC core, it is a 32 bit CPU core. But at meanwhile, P4080 support 36bit address.

So, my questions is how to use these address space beyond 4G(since 32 bit CPU only can initiate at most 4G address)?

Could you please share some doc with me? Thanks a lot!

Labels (1)
0 Kudos
1 Reply

262 Views
ufedor
NXP Employee
NXP Employee

Please refer to the AN4064 - Utilizing 36-Bit Physical Addressing in U-Boot and Linux:

http://cache.nxp.com/files/32bit/doc/app_note/AN4064.pdf?fsrch=1&sr=1&pageNum=1

0 Kudos