SDK v2.0, linux-ls1 4.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK v2.0, linux-ls1 4.1

628 Views
xkonni
Contributor II

Getting started with a LS1021a board, building images with yocto, so far it works as expected.

we got a binary kernel module from a partner, compiled with the SDK v2.0 for a 4.1.8 kernel.

Unfortunately it was built with other flags than the kernel packaged with the SDK and won't load.

Also the packaged kernel has serious network driver issues, resulting in crashes.

So i'm trying to recompile linux-ls1 4.1.8, but can't find appropriate sources, maybe you could point me in the right direction.

Thanks for your help!

Labels (1)
Tags (1)
0 Kudos
1 Reply

491 Views
xkonni
Contributor II

found it. it's the sdk-v2.0.x branch here: git://git.freescale.com/ppc/sdk/linux.git

unfortunately the ethernet driver shows the same crashes like the kernel image included in the sdk download.

see https://community.nxp.com/message/672293#comment-672293

0 Kudos