Content originally posted in LPCWare by bhallett on Mon Mar 22 07:57:43 MST 2010
Hello All,
I have a requirement to setup the Internal 32 bit timer0 and an external GPIO port interrupt to the same interrupt priority (the highest) on a LPC1342 processor, does anyone know if this is possible using NVIC_SetPriority i.e.
NVIC_SetPriority(EINT0_IRQn,0);
NVIC_SetPriority(TIMER_32_0_IRQn,0);
Or, does some other method have to be used.
Regards
Barry