Content originally posted in LPCWare by micrio on Mon Feb 13 05:50:31 MST 2012
There seems to be a bug with the Program Flash tool.
If I use the "Program flash memory" tab, select the file to flash, and select the "Mass erase" option. The file appears to be written to flash OK but the flash is not erased entirely. Stuff that my app has written at the top of the flash address range using IAP is not erased.
If I use the "Erase flash memory" tab then all of flash is erased as expected.
Do the settings in the Program Flash tool affect the debug tool when it programms flash?
Thanks,
Pete.