Content originally posted in LPCWare by frame on Fri Feb 17 04:39:20 MST 2012
At least it work now with the 8-Bit parallel interface - one should read all the documentations REALLY carefully.
Since the SD1289 datasheet states that D1...D8 is used in 8 Bit mode, I wired D1 ...D8 on the QVGA board connector to the GPIO port. I failed to notice, however, that D0 of the controller was not routed to D0 on the connector, but used otherwise. D1...D8 of the controller were already routed to D0...D7 on the external connector. Thus I connected GPIO port effectively to D2...D9, which did of course not work.
For the LPCXpresso1769, I tried the OLED example for the LPCXpresso-Baseboard, which worked out of the box (well, almost).
This example uses SPI by default, the routines come from an EA library (Lib_EaBaseBoard, which is part of the example workspace for Baseboard/LPC17xx).
Since serial readout is not supported by the QVGA LCD controller anyway, I'm not following this route anymore.