lpcware

How to run a project on LPCXpresso1769?

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by Damien1232 on Tue Nov 24 09:38:35 MST 2015
Hi,

I use CLEV663B board (CLRC663 reader board and LPCXpresso1769 board) . My CLRC663 reader board is configurated to run in UART.
I would like to know how to run a project that is describe in this document (http://www.nxp.com/documents/application_note/AN11211.pdf).
I follow steps but I don't understand why it doesn't work.
After importation of the librairy (attached file). I Debug NfcrdlibEx5_ISO15693 for example and I click on the button resume.
I get this text in the console window:

*** ISO 15693 Example ***

Reader chip RC663: 0x18

Ready to detect


I haven't got error message, and the board doesn't detect any RFID tags

If anyone has a hint, I would appreciate

Original Attachment has been moved to: CLEV663B-LPC1769_NFC-Reader-Library-v3.092_0.zip

Outcomes