lpcware

LPCXpresso 4.0.5 [113] fails to start on Fedora 15

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by pabloridolfi on Thu Jun 30 06:45:51 MST 2011
Hello,

I'm trying to run LPCXpresso IDE 4.0.5 [113] on a Fedora 15 system.
When starting, the splash screen appears but throws the following exception:

#
# A fatal error has been detected by the Java Runtime Environment:
#
#  SIGSEGV (0xb) at pc=0x9769ca07, pid=2400, tid=3077580480
#
# JRE version: 6.0_18-b07
# Java VM: Java HotSpot(TM) Client VM (16.0-b13 mixed mode linux-x86 )
# Problematic frame:
# C  [libxul.so+0xc84a07]
#
# If you would like to submit a bug report, please visit:
#   http://java.sun.com/webapps/bugreport/crash.jsp
# The crash happened outside the Java Virtual Machine in native code.
# See problematic frame for where to report the bug.
#

It seems to be a memory problem, so I increased the amount of memory allocated by eclipse, specified in the lpcxpresso.ini file, but the problem remains.

The complete log file is attached.
Thanks in advance for any advice.

Regards from Argentina.
Pablo

Outcomes