Content originally posted in LPCWare by Rob65 on Mon Jul 02 13:46:38 MST 2012
What is the behaviour that you are looking for?
"half bridge PWM with dead time" sounds like two PWM outputs with one output being high for a certain time, followed by a 'dead time' (no outputs high) and then the next PWM being high.
If that is the case, re-read your user manual for the timer operation. As I read it, the timer's PWM outputs are single edge PWMs. If you need double edge PWM signals the you might want to get an LPC1xxx variant that has a MCPWM block for motor control.
What do you want to do with the buck converter? You do realize that you need a fast control loop to measure and adjust your PWM settings, otherwise your voltage will run away.
I tried to do something like this for high power LEDs but stopped my attempts after the first simulation runs.
Rob