Content originally posted in LPCWare by jx1 on Mon Jun 03 19:22:44 MST 2013
Hi everyone,
I encountered some problems trying to use the DaliController to control the brightness of the lamp. I am using the LPCXpresso v5.2.4 This is what I have done : Firstly, I import the CMSIS library of LPC1343. After that,I create a new project;add in the header and source files for dali master. I compile the program and debug.Then I use the usb to supply voltage to the dali master but it could not control the brightness of the lamp. Is it due to the binary code ? My binary code which I generate is 6KB compared to the one provided by dali software development kit which is only 2KB.