lpcware

Batch file not auto closing with crt_emu_lpc11_13_nxp and LPC Link2

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by clayton on Tue Sep 23 09:27:26 MST 2014
We always used the Red Probe+ with Code Red Suite until the Red Probe+ was discontinued. Now we are using the LPC Link2 programmer with LPC Xpresso (crt_emu_cm_redlink for command line batch programing). My batch file has the following commands which are working fine.

C:\nxp\LPCXpresso\lpcxpresso\bin\crt_emu_cm_redlink -pLPC11C14/301 -vendor=NXP -vc -flash-load="BINs\xxxxxxxxxxx.bin" -load-base=0x6000
C:\nxp\LPCXpresso\lpcxpresso\bin\crt_emu_cm_redlink -pLPC11C14/301 -vendor=NXP -vc -flash-load-exec="FW\DisplayApp.axf"

All I want to do is have the command window automatically close done once programing is complete. We had no issue with this using crt_emu_lpc11_13_nxp from the code red suite (using the Red Probe+). What command or argument can be added so that my command window automatically closes upon completion of the second upload?

Outcomes